Access and Run a Registry Editor
On occasion, you may need to make changes to Geo SCADA Expert's settings directly in the registry in Windows®. The settings are stored in a small section of the registry, clearly marked as 'Geo SCADA Expert'. Many of Geo SCADA Expert server’s settings are configurable using the Geo SCADA Expert Server Configuration Tool. For other Geo SCADA Expert settings, you may have to use a Registry Editor, such as Regedit. This topic provides guidelines on how to access Regedit. The means by which you access the Registry Editor varies, depending on the operating system. For operating systems not mentioned in this topic, please refer to your Windows documentation.
Windows 10
To access the Registry Editor:
- Type
regeditin the Search box next to the Start menu in Windows, and then press the Enter key.
The Registry Editor is displayed.
To access the Registry Editor:
- Select the Start button on the Windows taskbar.
- Select the All Programs option, followed by the Accessories option.
- Select the Run entry.
The Run window is displayed. - Enter the following text in the Open field:
regedit

- Select the OK button.
The Registry Editor is displayed.
INOPERABLE DEVICE